Press Releases
Motion plastics leader sees 30 percent online growth amid worldwide pandemic June 24, 2021 – An increase in the pace of innovation and emphasis on expanding its digital presence in the face of a worldwide pandemic helped igus increase online sales by 30 percent in 2020. Innovations range from telescopic robot tube packages to dry-running […]
The judges recognize four unique projects for their use of self-lubricating, polymer bearings Four times the excitement: for the first time, the manus award, a joint initiative by igus, a motion plastics specialist, recognises four contestants. The prize showcases fascinating, creative uses of plain bearings. The tenth gold manus award goes to Kässbohrer Geländefahrzeug AG […]
Self-lubricating and maintenance-free heavy-duty material iglide TX2 shows a 3.5-fold improvement in wear tests June 8, 2021 – igus has introduced a new bearing with an improved iglide material, TX2, which offers self-lubricating and maintenance-free properties for heavy duty applications. TX2 increases wear-resistance by a factor of 3.5 in load ranges with more than 100 […]
HydroPRS pioneer Mura Technology begins construction of the world’s first commercially operated hydrothermal upgrading plastic recycling plant in the UK April 12, 2021 – Plastic waste that would otherwise pollute the environment can now be reused as a valuable raw material through a 25-minute chemical recycling process. igus, the Germany-based motion plastics specialist, is helping […]
igus components help New York designer create easy-to-install product March 17, 2021 – Newly-developed hands-free door openers by a New York City-based design company make the task easier while also providing an affordable, easy-to-install device that promotes contactless, sanitary-safe entry. The patent-pending hands-free openers from MYT Wares in Brooklyn include components from igus, the Germany-based […]
New slip ring-free igus cable unwinder allows easy cable management February 9, 2021 – igus has developed the e-spool® flex 2.0, a new cable reel that has no slip ring that is perfect for industrial robot users. This allows for easy management of robot teach pendants and the system even supplies bus signals without interruptions, […]
The manus award celebrates its tenth anniversary and introduces its first sustainability prize JANUARY 26, 2021 – Nominations are open for the manus award from igus, which honors extraordinary and unique use of the company’s high-performance plastics in product design. The winner will receive prize money of up to 5,000 euros. To mark the tenth […]
igus introduces E4Q, a lightweight e-chain for unsupported lengths and long travels September 30, 2020 – igus introduced its E4Q energy chain, which offers a smooth, contoured design and a completely new crossbar concept with weight-reducing locking straps. The new design ensures that the e-chain can be opened and closed in seconds without tools. The […]
With the online service life calculator, users can now determine the guaranteed operating time of their e-chain and obtain a certificate September 24, 2020 – igus now offers a 36-month guarantee on its energy chains, which are in demand for a wide range of job applications. The robust, lightweight, and long-lasting energy chains are made […]
New solution gives UR and robolink units dramatically increased action radius September 16, 2020 – igus now offers a ready-to-connect 7th axis that will allow a robot to move over a distance several meters and includes a maintenance-free drylin ZLW toothed belt axis with a corresponding adapter plate, switch cabinet, cables, and software integration. For […]