Application Stories
Autonomous cleaning robot runs even cleaner with drylin linear bearings Self-lubricating drylin® linear guides ensure smooth operation of the K900 cleaning robot from KEMARO AG The K900 industrial robot cleans floors wherever it needs to, autonomously and without programming, even in places where it is potentially dangerous or even impossible for people to clean. Self-lubricating linear guides, shafts, plain […]
Maintenance-free special plain bearings from igus as a fast and economical solution for recumbent bikes by ergoline GmbH Ergometers are not only popular in gyms or as exercise machines at home; they are also used in medical technology for diagnosing heart diseases. One of the leading manufacturers of ergometers is ergoline GmbH. The company’s tilting-recumbent […]
The Linkage System gives the A-Frame made by Ship & Yacht Engineering a 180-degree range of motion Founded in 2000, Ship & Yacht Engineering Limited specializes in managing and implementing complex shipbuilding and marine technology projects. Its founder and CEO, Erik Hofmann, develops everything needed in shipbuilding, from ramps to cruise ships. While working with […]
Roboeatz is revolutionizing the food service industry by relying entirely on igus motion plastics, which require no lubrication or maintenance. The Canadian start-up Roboeatz has developed a kitchen where a robot is the only cook! The robot chef quickly and efficiently makes a wide range of dishes from fresh ingredients. In developing this unique robot cell […]
Who says automation has to be expensive? In Bruges, Belgium, the chocolate shop Roose’s Chocolate World has a robot called Chocomatic built at a bargain price. It packs chocolates in front of customers. A robolink® robot from igus® is used, which moves on a seventh axis. A customer enters Roose’s Chocolate World at Havenstraat 1 in Bruges. […]