ReBeLMove Pro: modular robot platform for logistics, assembly and handling

Autonomous mobile robot from igus promises simple configuration with flexible superstructures and easy commissioning

The ReBeLMove Pro acts as a versatile base for multiple add-ons, including order-picking systems, smart shelving units, and collaborative robots equipped with conveyor belts. (Source: igus GmbH)

Pressure in terms of costs and efficiency demands a lot from modern production. With the ReBeLMove Pro, igus is launching a modular autonomous mobile robot (AMR) that is easy to customise according to the modular principle – from small load carrier transport to robot solutions. It can be integrated into company processes without any previous experience. The ReBeLMove Pro is available from just €39,800, which makes it around 25 per cent more cost-effective than most competitor models.

The ReBeLMove Pro is based on a compact, rectangular transport robot on four wheels with an electric drive. The AMR is 795mm long, 560mm wide, 195mm high, weighs 60kg and is painted in black with orange accents typical of igus. The robot can navigate autonomously at a speed of up to 2m/s, carry up to 250kg or pull up to 900kg in material handling. One battery charge is enough for a full working day of eight hours. By adding attachments to the ReBeLMove Pro, users can adapt it to different tasks in material handling. Examples include height-adjustable conveyor belts and an articulated arm cobot for assembly workstations, a trailer for transporting materials or a shelf with light signals for more productive order picking. The new robot can also be used outdoors. “igus itself is already using the ReBeLMove Pro as a shuttle to transport products away from injection-moulding machines in production,” says Sebastian Thorwarth-Kienbaum, Expert for Low Cost Automation at igus. “These are tedious, routine tasks in material handling that companies find difficult to get people excited about.” Within just two months, for example, a fully automated container transport system including interface integration was realised in igus’s production, from conception to implementation. It transports ball bearing components from the injection-moulding machine to the fully automatic assembly machine without human intervention.

ROI in Just 12 Months

Savings extend beyond purchase price. “System integrators and software licenses often cause high follow-up costs, which lead to companies putting the topic of automation on ice again in frustration,” says Thorwarth-Kienbaum. “We have therefore made a point of ensuring that the ReBeLMove Pro can be integrated and operated without outside help or automation experience.”

During a simple round trip, the robot creates a 3D digital map using LIDAR, 3D sensors, and a RealSense camera—mapping 200 m² in under three minutes. Programming is intuitive: users can set up movements in 15 minutes without coding skills. Integration with IT systems via open interfaces (IoT, VDA 5050, REST, SAP, ERP) is straightforward, and the AMR works with fleet management tools like Fleetexecuter, Kinexon, and Naise.

“Thanks to the low investment costs and uncomplicated commissioning and operation, the average return on investment for a ReBeLMove Pro is twelve months. The ReBeLMove Pro costs only €38,900, i.e. around 25 per cent less than standard market solutions, which generally start at €50,000—without compromising on functionality,” summarizes Thorwarth-Kienbaum.

You may also like...