New two-component bushing stands tough in extreme conditions
iglide Q2E from igus tested to withstand loads up to 130 MPa
August 14, 2019 – igus has developed a new lubrication-free, two-component bearing, iglide Q2E, that can withstand the extreme conditions frequently found in agricultural machines, utility vehicles, offshore installations and other demanding environments.
The new bushing ensures a high-degree of wear-resistance and a hard polymer shell protects the heavy duty bearing. In tests at the company’s expansive test laboratory, the new material withstood loads up to 130 MPa.
igus, the Germany-based manufacturer of motion plastics, runs its North American operations out of Providence, R.I.
Need for durable materials
Bearings in construction equipment, agricultural machines and offshore installations have difficulty coping with the extreme conditions encountered in these rugged industries. Dirt, impact and high edge loads cause premature wear. In these scenarios, durable materials and dirt-resistant components are required to meet the challenge. The new iglide Q2E bearing is designed for such situations.
Expensive central lubrication systems are no longer necessary. Dirt and impurities can no longer adhere to the bearing points, which minimizes wear. In addition, less grease and oil escapes into the environment. As a result, the annual consumption of more than 35 million metric tons of lubricant, as measured by RWTH Aachen University, is reduced.
Another advantage of the new bearings is that the injection-moulding method used to manufacture them is extremely cost-efficient.
The combination is the secret
Two materials in an encapsulated design ensure that the bearing can cope with the most extreme edge loads. The iglide Q2E has a hard polymer shell and a tribologically optimized core composed of iglide Q2 as the material. When used for a plain bearing with a diameter of 20 millimeters, the material is also dimensionally stable and wear-resistant, even under high loads of up to 7 metric tons.
Functioning as a protective sheath, the shell makes the bearing quite sturdy and ensures that it has a longer service life. In a swivel test in the igus test lab, the material withstood a radial load of 130 MPa.
iglide Q2E is initially available for shaft diameters of 20, 25, 30 and 40mm. For more information on the full array of igus products, visit www.igus.com/product/701